AXIS#.BODE.PRBDEPTH
Description
AXIS#.BODE.PRBDEPTH sets the length of the PRB signal before it repeats. This applies only when AXIS#.BODE.MODE = PRB. The PRB excitation will repeat after (2^AXIS#.BODE.PRBDEPTH) / AXIS#.BODE.EXCITEGAP drive samples.
Example
Set AXIS1.BODE.PRBDEPTH to 19:
-->AXIS1.BODE.PRBDEPTH 19
Get AXIS1.BODE.PRBDEPTH (already set to 19):
-->AXIS1.BODE.PRBDEPTH 19
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
NA |
|
Range |
4 to 19 |
|
Default Value |
19 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.BODE.PRBDEPTH | 0x5001 | 0x2 | USINT | - | - | RW | False |
| AXIS2.BODE.PRBDEPTH | 0x5101 | 0x2 | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|